Please note that this documentation was originally released for the CRD300DA12E-XM3, but it also supports the CRD250DA12E-XM3 and the CRD200DA12E-XM3. The only difference between these three versions of the XM3 reference design are the configuration of the half-bridge module populated. The part numbers correspond as follows:
	CRD300DA12E-XM3 = 3 CAB450M12XM3 Modules
	CRD250DA12E-XM3 = 3 CAB425M12XM3 Modules
	CRD200DA12E-XM3 = 3 CAB400M12XM3 Modules

If you see a reference in this documentation to the CRD300DA12E-XM3 or CAB450M12XM3, but you have purchased a different part number, please understand that it is referring to the inverter / module platform generally.

For any performance-related questions, defer to the appropriate module or gate driver datasheet / application note, as appropriate. If you have any questions, please contact Wolfspeed.

Thank you for using the XM3 power module platform, we're excited to see how you use it!